ACTION#.SOURCEID

Description

Some action sources require a specific source ID number. For example, if your action source is a Digital Input, then a source ID of 1 would correspond to Digital Input 1.

The range of the source ID will depend on the value of the corresponding source. If the source is modified, the range and units of the source ID may change, and the source ID value will default to the first valid value.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Depends on ACTION#.SOURCE

Range

Depends on ACTION#.SOURCE

Default Value

0

Data Type

Integer

Stored in Non Volatile Memory

Yes

Variants Supported

All variants are supported

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen